IP.RESET

Description

This command is used to acquire a new IP address for service port communication based on which IP.MODE is specified.

Examples

Usage

After making changes to IP parameters, IP.RESET can be used to acquire a new IP address. When the command is issued, the drive will disconnect from Workbench. IP.RESET will return an error if the command is issued while an axis is enabled.

Code

Set drive to use static IP of 192.168.0.1

--> IP.MODE 1
--> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.RESET

Context

For more information on IP configuration, refer to Finding and Connecting to a Device.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Command
Units N/A
Range N/A
Default Value N/A
Data Type N/A
See Also IP.MODE, IP.ADDRESS, IP.SUBNET, IP.GATEWAY

Stored in Non Volatile Memory

No

Variants Supported

All variants supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen